LPC1857- Revision changes 'A' vs '-'- Impact on sleep and reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1857- Revision changes 'A' vs '-'- Impact on sleep and reset

1,494件の閲覧回数
vivienwong
Contributor I

Hi,

   I have 2 LPC1857 chips with different device revision:

1. ESD14440- (initial device revision)

2. ESD16030A (second device revision)

   I noticed that there is a different between the 2 device revision whereby when both are put into DeepPowerDown low power mode, the nRESET button would wake the ESD14440-  up but not the ESD16030A.  My workaround now is to use the event router bit 19 to detect low level of RESET_SETEN to wake the chip up (ESD16030A).

   What has changed between the 2 device revisions? Is there an errata to explain the differences between the 2 device revisions?

ラベル(1)
0 件の賞賛
返信
1 返信

1,345件の閲覧回数
thefallguy
Contributor IV

Searching for "LPC1800 errata" will provide the document you are looking for...

0 件の賞賛
返信