LPC1857 Ethernet FBI (fatal bus error) reading tx descriptor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1857 Ethernet FBI (fatal bus error) reading tx descriptor

1,653 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Grant.Edwards on Thu May 09 16:48:05 MST 2013


I'm trying to use the Ethernet controller on a Keil LPC1857 eval
board.


After setting up descriptor arrays, buffers, configuring MAC and DMA,
I get a fatal bus error indicated in the DMA status register
immediately on setting the DMA_OP_MODE ST bit.  I've verified that
DMA_TRANS_DES_ADDR is pointing to a descriptor, and after the error
occurs DMA_CURHOST_TRANS_DES looks valid.  Here's waht I end up with
in DMA status


<code>
DMA_CURHOST_TRANS_DES = 0x0000e308
DMA_OP_MODE = 0x00002008
DMA_STAT = 0x03802002
   TI 0
  TPS 1
   TU 0
  TJT 0
  OVF 0
  UNF 0
   RI 0
   RU 0
  RPS 0
  RWT 0
  ETI 0
  FBI 1
  ERI 0
  AEI 0
  NIS 0
   RS 0
   TS 0
  EB1 1
  EB2 1
  EB3 1
</code>


I've got 16MB of SDRAM starting at address 0, and
the address for the current tx descriptor (0xe308) is correct.


What are possible causes of the fatal bus error when the DMA
controller is reading a tx descriptor?

标签 (1)
0 项奖励
回复
1 回复

1,631 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Grant.Edwards on Fri May 10 08:48:15 MST 2013

The M3MEMMAP feature that is used to map SDRAM to address 0x00000000 doesn't affect the DMA controller, so the descripter and buffer pointers are invalid.


Translating them to unmapped addresses (in this case 0x2800xxxx) when setting up the descriptors and configuring the DMA controller fixes the FBI problem.

0 项奖励
回复