LPC1850EVA RevA4 hitex SDRAM @ 120Mhz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1850EVA RevA4 hitex SDRAM @ 120Mhz

1,063 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by benravin on Wed Apr 04 02:34:45 MST 2012
Hi,

We are  facing an issue with SDRAM(IS42S16400F) on Hitex board LPC1850EVA-A4. If  run with 72MHz clock then  data write/read from SDRAM is correct. But If  increased to 120MHz the data write/ read is not correct.

The clock is increased to 120MHz by setting the PLL1 using API  “CGU_SetPLL1(10)”  in CGU_Init() function.

Please help in resolving this issue.

Tools:
Red Suite:
Version: Red Suite v4.2.0 [Build 349] [25/02/2012]

Regards,
Biju
标签 (1)
0 项奖励
回复
1 回复

1,041 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by PhilYoung on Wed Apr 04 13:22:44 MST 2012
presumably you did the PLL update before setting up the SDRAM controller, since the example setup code uses the current operating frequency to compute the timing parameters for the SDRAM interface.
0 项奖励
回复