LPC1837 Boot ROM mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1837 Boot ROM mode

1,853 Views
ethanchen
Contributor II

Hi all,

I check LPC1837 datasheet page 63 about boot ROM have related description for Mass Storage Class

ethanchen_0-1599787160897.pngethanchen_0-1599787160897.png

Setting Boot source bit pin to USB0 or USB1?

ethanchen_1-1599787389380.pngethanchen_1-1599787389380.png

How to perform MSC boot?

Thank you.

Best Regards,

Ethan Chen

0 Kudos
Reply
1 Reply

1,833 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ethan,

The "MSC" means that the USB module of LPC1837 can be enumerated as a disk driver after it is plugged into PC so that you can drag the *.bin file to the disk driver, the *.bin file will be saved into on-chip flash. If you set the P2_9/P2_8/P1_2/P1_1 as low/high/low/high, if you enter ISP mode by setting P2_7 as low during/after Reset, can you see the disk driver after you insert the USB0?

Anyway, I suggest you download the latest Flash Magic tools from the link:

https://flash-magic.informer.com/download/#downloading

The tools can detect the USB automatically, pls try to download application code via USB with the tools.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply