LPC1833 EEPROM reading

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1833 EEPROM reading

跳至解决方案
1,773 次查看
michaelershov
Contributor I

Hello, 

If I store important information in EEPROM; Flash protected from reading. Anyone can erase only Flash and write new code for reading EEPROM?

 

Best regards

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,483 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Michael Ershov,

In general, the Flash and EEPROM are independent peripherals, if the enable code read protection don't interfere the EEPROM operation.

So it's available to achieve your purpose.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,484 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Michael Ershov,

In general, the Flash and EEPROM are independent peripherals, if the enable code read protection don't interfere the EEPROM operation.

So it's available to achieve your purpose.
Have a great day,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复