LPC1830-Xplorer as demo for a custom USB device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1830-Xplorer as demo for a custom USB device

561 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by samuele on Mon Jun 03 02:53:09 MST 2013

Hi,


I'm at my first tries with Cortex-M and USB. I have the need to build an USB device that should be able to interface with an SPI device that outputs data at around 1MBps. This USB device should be a device that could permit a user to control from a PC, the SPI device and read the data from the SPI device. Moreover the data outputted from the SPI device should be saved on an SD card (that should be accessible through USB).


Just to be clear, the layout should look like this:


[ PC ]-------USB-------[ MY_CUSTOM_DEVICE ]---SPI---[ SPI_DEVICE ]


                                              |


                                              +---- [SD_CARD]


 


My requirements are:


- control the SPI device with a PC through the USB


- read the data produced by the SPI device (1MBps) with a PC through the USB


- store the data produced by the SPI device on an SD card


- access the SD card with a PC through USB


 


I was thinking of using the LPC1830-Xplorer board as a demo board to start developing the firmware.


Given that I'm at my first USB device project, I'm looking for feedbacks/opinions/suggestions if it's possible to satisfy all the requirements with this hardware.


 


Thanks for any suggestions.


 


Regards,


Samuele.

Labels (1)
0 Kudos
Reply
0 Replies