LPC1830 NGX board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1830 NGX board

2,003 Views
jan92
Contributor II

Hello,

I need to upload my program into internal flash memory in LPC1830, not spifi. When I try to do it then the LPCxpresso returns this error Ef (34): Timed-out initializing flash.

Iam using the LPC18x7_43x7_2x512_BootA.cfx flash driver.

Anyone knows where can be the problem?

Labels (1)
Tags (4)
0 Kudos
Reply
1 Reply

1,494 Views
lpcxpresso_supp
NXP Employee
NXP Employee

The problem is the fundamental one that LPC1830 doesn't have any internal flash. This is what the "0" indicates in the last digit of the part number.

If you want internal flash, you will need to use a part such as the LPC1837 or LPC1857. For more details please see the LPC18xx user manual and data sheet (LPC1800 32-bit MCUs|ARM Cortex-M3 Cores|NXP), and for LPCXpresso IDE related information on LPC18 flash drivers see:

LPC18xx / LPC43xx Internal Flash Drivers

LPC18xx / LPC43xx SPIFI Flash Drivers

Regards,

LPCXpresso Support

0 Kudos
Reply