LPC1830+JLINK+OpenOCD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1830+JLINK+OpenOCD?

1,128 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by TimucinAnuslu on Thu Feb 27 14:55:10 MST 2014
Hi all,

I use JLINK and OpenOCD as debugger and flasher. I connect to LPC1830-XPLORER with both these and LPC1850 config of OpenOCD. (I cannot find LPC1840 config for OpenOCD) And then reset and halt commands run successfully. But I cannot write a binary file or elf file. Which command can I use to program external quad flash?

Thanks
Labels (1)
0 Kudos
Reply
1 Reply

1,059 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Thu Feb 27 16:14:58 MST 2014
purchase the $20 LPC-Link-2
I do not think OpenOCD is supported.  You might get it to work if you google for settings, but ...
0 Kudos
Reply