LPC1817 SPI Clock delay issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1817 SPI Clock delay issue

ソリューションへジャンプ
2,086件の閲覧回数
chase_lin
Contributor I

I got SPI clock issue in SPI 8 bits mode. Does anyone know any configuration for reducing delay of clock ? I would like to make clock continuously. Thanks.

chase_lin_2-1630487025869.pngchase_lin_2-1630487025869.png

 

スポイラ
SPI


 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,066件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, there is no register for configuring delay between transfers. Is SSEL pin kept low between transfers? Please not that if you are using SPI format with CPOL=0,CPHA=0 requires SSEL set to 1 between transfers in continuous transmission.

Best regards,

Felipe

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,067件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, there is no register for configuring delay between transfers. Is SSEL pin kept low between transfers? Please not that if you are using SPI format with CPOL=0,CPHA=0 requires SSEL set to 1 between transfers in continuous transmission.

Best regards,

Felipe

0 件の賞賛
返信