LPC1817 SPI Clock delay issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC1817 SPI Clock delay issue

跳至解决方案
2,069 次查看
chase_lin
Contributor I

I got SPI clock issue in SPI 8 bits mode. Does anyone know any configuration for reducing delay of clock ? I would like to make clock continuously. Thanks.

chase_lin_2-1630487025869.pngchase_lin_2-1630487025869.png

 

破坏者
SPI


 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,049 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, there is no register for configuring delay between transfers. Is SSEL pin kept low between transfers? Please not that if you are using SPI format with CPOL=0,CPHA=0 requires SSEL set to 1 between transfers in continuous transmission.

Best regards,

Felipe

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,050 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi,

Unfortunately, there is no register for configuring delay between transfers. Is SSEL pin kept low between transfers? Please not that if you are using SPI format with CPOL=0,CPHA=0 requires SSEL set to 1 between transfers in continuous transmission.

Best regards,

Felipe

0 项奖励
回复