LPC17xx suspend watchdog in sleep

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC17xx suspend watchdog in sleep

680 Views
laurianussss
Contributor II

I have a problem with LPC1768 controller. I want to use an watchdog to reset controller if stucks. 

I also want to use deep sleep. 

Problem appears when i want.to use both. If I enable watchdog as i saw there is mo possibility to suspend or disable so when system enter in deep sleep watchdog will reset the controller as it is not feed anymore.

Any solution to disable somehow watchdog when enter in sleep mode or other solutions to work both (deep sleep and an watchdog to reset mcu if stucked?)

A solution i am thinking is to use a timer with highest priority and reset in this timer is higher than a value. Value will be reset in while loop in main. I do not know if this one Will work OK 

 

 

 

 

0 Kudos
Reply
3 Replies

656 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @laurianussss 

 

It requires a hardware reset or a Watchdog reset/interrupt to
be disabled.

 

BR

Alice

0 Kudos
Reply

651 Views
laurianussss
Contributor II

How can i disable watchdog IRQ/Reset? As I have read in data sheet it says it cna not be disbaled in software once it is enabled. Only an hardware reset will do it.

Thanks

Laurian

0 Kudos
Reply

630 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @laurianussss 

Yes, once the watchdog of the LPC1768 is enabled, it cannot be disabled via software.

Yes, you can consider using a timer to wake up the MCU and feed the watchdog. Alternatively, you can consider using an external watchdog IC.

 

BR

Alice

 

0 Kudos
Reply