LPC17xx hardware design bug in DMA engine ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC17xx hardware design bug in DMA engine ?

1,579件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thedaz on Thu Apr 14 00:57:18 MST 2016
There have been multiple reports of the DMA failing to operate properly unless the target memory area lies in RAM2. The symptom is not visible during debugging but only when the controller is run standalone. So far NXP hasn't made a single attempt to explain why the DMA works reliably with RAM2 but not with the standard RAM area so the only conclusion left (for me) is that NXP is aware of a design bug doesn't want to admit.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,545件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信

1,545件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by thedaz on Fri Apr 15 01:00:16 MST 2016
As long as there's not even a response from NXP they're not better.
0 件の賞賛
返信

1,545件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rocketdawg on Thu Apr 14 06:51:00 MST 2016
Nah,
NXP is pretty good at publishing errata.  They have little reason to deliberately hinder their customers.
They probably have not yet qualified and verified under what circumstances the issue appears.
you want to see some messed up parts, just look at the errata for some MIPS based hardware !!!
0 件の賞賛
返信