LPC17xx and LPC40xx LPCOpen v2.10 packages released

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC17xx and LPC40xx LPCOpen v2.10 packages released

1,605 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by NXP_Support on Wed Mar 12 17:00:28 MST 2014
The new LPCOpen packages for the following boards are available at LPCOpen page.

LPC17XX Boards
- EA DevKit 1788
- NXP LPCXpresso 1769

LPC40XX Boards
- EA DevKit 4088

For more information on changes visit the change log page at change history page.
Labels (1)
0 Kudos
Reply
3 Replies

1,538 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by schisanoa on Tue May 13 09:02:53 MST 2014
Has anyone successfully tested SDMMC example with  EA DevKit 4088??

I can't test the example code because it doesn't work
0 Kudos
Reply

1,537 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ozenozkaya on Tue May 06 02:13:44 MST 2014
We have written the PWM0/1 drivers for the LpcOpen platform. You can see this topic:
http://www.lpcware.com/content/forum/lpcopen-pwm-driver
0 Kudos
Reply

1,538 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by YOZHik on Fri Apr 11 06:12:59 MST 2014
Any plans to add support for LPC178x/7x Pulse Width Modulators (PWM0/1) to the package?
0 Kudos
Reply