LPC17xx + SDRAM 8Bitsbus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC17xx + SDRAM 8Bitsbus

1,343件の閲覧回数
kittanadon_aek
Contributor I

Dear all,

I'm developing 

LPC1778FBD208 interface with MT48LC16M8 (16Mx8) how i can config SDRAM  in 8Bits ?

LPC17xxx‌

Thank you

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,082件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Kittanadon Keawratchakit,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd like to suggest you refer to these two application notes to learn how to interface the SDRAM to LPC MCU.

https://www.nxp.com/docs/en/application-note/AN11508.pdf

https://www.nxp.com/docs/en/nxp/application-notes/AN12026.pdf
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信