LPC17xx SD Control with SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC17xx SD Control with SPI

2,002 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yasinidz on Wed Dec 19 08:35:23 MST 2012
hi,
I have founded some examples using SD interface to access SDCard. Are there any examples using SPI for LPC1788? if the example includes EFSL or Chan Fatfs, it can be more usefull for me. Thanks for help.
Labels (1)
0 Kudos
Reply
3 Replies

1,907 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by varnit on Tue Nov 04 21:36:24 MST 2014
Can we use this library for LPC1857 also. with minor changes
0 Kudos
Reply

1,907 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by yasinidz on Thu Dec 20 00:45:14 MST 2012
infact I dont want to lose time with "sending commands and getting responses" part. I need an example that includes these (init, send, read and run stable)for SPI. Can I find any or i'll start to write my own. But i know there are many users who has already wrote these parts for SPI mode. I thought that can make my job easier with small modifies on code.  
0 Kudos
Reply

1,907 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Lien.Nguyen on Wed Dec 19 20:45:23 MST 2012
You can refer to http://www.lpcware.com/content/nxpfile/an10916-fat-library-efsl-and-fatfs-port-nxp-lpc1700. It is for LPC1768 but I think it won't take much time to change to LPC1788.

Best Regards,
Lien
0 Kudos
Reply