LPC17xx RAM1 and RAM2 memory areas

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC17xx RAM1 and RAM2 memory areas

1,274 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cybersteve on Tue Mar 29 07:19:38 MST 2016
I have run out of space in my LPC1768 32k RAM area. I would like to place variables (data buffers) in the other two 16k RAM areas.

I am using the ATOLLIC IDE (no code limit) which, I believe, is eclipse based.

I would like to find out the macro that would cause the compiler/linker to put this data in RAM1 or RAM2.

The expresso macros don't work

__BSS(RAM2), etc.


Help!

Thanks

Labels (1)
0 Kudos
Reply
1 Reply

1,202 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply