LPC17xx - Input PullUP / PullDown / Weak or Strong - Current values

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC17xx - Input PullUP / PullDown / Weak or Strong - Current values

1,481件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rnj on Mon May 25 14:54:36 MST 2015
Hello!!!

I'm looking for the values of the weak pull-ups when the LPC1768 is on default state. Looking on datasheet I found values for current on theses pins, Ipd and Ipu, but the datasheet doesn't make it clear if these values are for strong or weak PU/PD.

Another doubt is that in the page 75 the diagram show the Pin schematic and the source of the PU/PD are VDD, but in the page 20 the note [1] there is another information about pull-ups values of 2.3V to 2.6V. I measured this same value in my Board.

Are these values right? During the MCU reset these GPIOs are configured as Input Pull-up, so can I consider the "weak" configuration? These currents of Ipd and Ipu are for Weak or Strong PU/PD? Or should I consider the current showed in the page 55 on Fig 14? Which is right?

Thank you!
ラベル(1)
1 返信

1,296件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by LabRat on Mon May 25 15:15:09 MST 2015

Quote: rnj
...During the MCU reset these GPIOs are configured as Input Pull-up, so can I consider the "weak" configuration?



That are weak values for input...