LPC178x: UART 38400bps with 12MHz IRC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC178x: UART 38400bps with 12MHz IRC

992件の閲覧回数
giusloq
Contributor III

I need to create a RS485/UART communication link between LPC178X and SAMD20 MCU. The communication should be 38400bps.

The clock on SAMD20 is based on an external 32.768kHz crystal (XOSC32K) and DFLL in closed loop mode.

I'm wondering if it is possible to clock LPC178X with internal IRC 12MHz oscillator. The datasheet reports a precision of 1% (11.88-12.12MHz) over all the voltages and temperatures. It seems sufficient for UART communication that usually needs a maximum of 2% error.

ラベル(1)
0 件の賞賛
返信
1 返信

966件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

Hello @giusloq,
I understand that you would use the IRC as core source clock, it is possible, as mentioned in the chapter 1.2 called "Features", as shown in the next image:

Habib_MS_0-1744146716879.pngHabib_MS_0-1744146716879.png


Also, if you experience any issue do not hesitate to let me know
BR
Habib.

0 件の賞賛
返信