LPC1788FBD208 data logger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788FBD208 data logger

2,922件の閲覧回数
aut
Contributor I

I'm using the LPC1788 (exactly LPC1788FBD208) microcontroller to make a data logger system. Several analog signals are connected to LPC1788. The user can download the acquired data, by means of several ways:

1) Via GPRS (a GPRS module is connected to the USART0 serial port)
2) Via Ethernet (the remote control room reads the data using internet connection)
3) Via USB pendrive (when the USB pendrive is plugged, the LPC1788 automatically download in the pendrive the data)
4) Connecting the LPC1788 to a PC (laptop or other type of personal computer) via USB cable (in this case, the LPC1788 has to be seen as an external hard disk)

Could you tell me in your opinion if a similar system can work properly?

Thanks

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

2,610件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Nico,

I'm not sure I understand your question, have you already implemented this functionality? Are you looking for recommendations on how to achieve this? If you are looking for example projects for UART, Ethernet and USB host and Device I would recommend you to take a look to the LPCOpen package for the LPC1788 devices:

http://www.nxp.com/products/software-and-tools/hardware-development-tools/lpcxpresso-boards/lpcopen-... 

Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,610件の閲覧回数
aut
Contributor I

Hi Carlos,

thanks for your support.

I have not implemented yet the functionality described in my previous post. I want to know if the hardware features of LPC1788FBD208 device allow to make these functionality.

Regards

Nico

0 件の賞賛
返信

2,610件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Nico,

 

Yes, the hardware features support the interfaces you are looking for. Regarding the memory, I have done a quick evaluation and it should be able to fit you application. The application sizes in dec are:
Data logger - periph_sdmmc 42580
Uart - periph_uart_rb 10668
Ethernet - lwip_tcpecho_sa 64636
USB Host - lpcusblib_MassStorageHost 59176
USB Device - usbd_lib_composite 16932

 

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,610件の閲覧回数
aut
Contributor I

Hi Carlos,

thanks a lot!

Where can I find the example projects that you indicated me in your previous response?

Regards

Nico

0 件の賞賛
返信

2,610件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Nico,

 

These are part of the LPCOpen package for the LPC1788 devices:
LPCOpen Software for LPC17XX|NXP 

 

Hope it helps!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信