LPC1788 to 4088 (Possible EMC issues)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 to 4088 (Possible EMC issues)

1,252 次查看
DiBosco
Contributor III

I have a board that has been cloned with minor changes from an LPC1788 to a LPC4088. It runs for a while and then falls over with a hard fault.

Reading this:

https://community.nxp.com/thread/419754 

It looks like there are minor changes when it comes to using the EMC (which we are). The set-up falls over when the LCD screen is being updated and the screen buffer is in external RAM, which leads me to believe there is every chance it is the SDRAM/EMC that is causing the issues.

However, I have been through each line of code and checked each register and I can see absolutely no difference whatsoever in the EMC registers between the two parts. Is anyone able to tell me what, exactly, the differences are in this respect between the two parts and what issues there might be?

Many thanks,

Rob

标签 (2)
0 项奖励
回复
1 回复

953 次查看
soledad
NXP Employee
NXP Employee

Hi,

Please check the AN11335 application note, this application note highlights some of the differences between these two families and provides guidance when switching from the LPC177x_8x based hardware/software to the LPC407x_8x systems.

http://www.nxp.com/docs/en/application-note/AN11335.zip 

I hope this helps


Have a great day,
Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复