LPC1788 sdcard interface drvie eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 sdcard interface drvie eMMC

2,282 Views
mini92
Contributor I

I use LPC 1788 SDIO interface driving eMMC but initialization err 

0 Kudos
Reply
2 Replies

1,965 Views
soledad
NXP Employee
NXP Employee

Hi,

According with the reference manual the LPC1788 supports SD card interface that also supports MMC cards only.
So, this device does not support eMMC.


Have a great day,

Soledad

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,965 Views
mini92
Contributor I

Hi,

    eMMC and MMC card Hardware interface is same ,different is driver software ,

 

   and MMC card drive  eMMC driver  The difference is very small

 

   Can software not support it?

I see

In fs_mci.c function :

/**
* @brief Read card configuration and fill structure CardConfig.
*
* @param None
* @retval TRUE or FALSE.
*/
Bool mci_read_configuration (void)

/* Select Card */
if(MCI_Cmd_SelectCard() != MCI_FUNC_OK) /* CMD7 tese same card reader */
{
break;
}

//  In this line add achieve:

EmmcReadExtCsd  

and according to ExtCsd message set same CardInfo

Can you help me?

thank you

0 Kudos
Reply