LPC1788 lcd display affect capture interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 lcd display affect capture interrupt

960 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by fire on Thu Sep 06 18:27:25 MST 2012
That the use of emwin516, display content by capturing the decoded, only capture a decoding display information, through the capture interrupt display information obtained is correct, as long as the information through the emwin516 interface function display out, capture interrupt is affected, one along the two times to capture interrupt, and capture register(CCR) value is the same as the capture the

标签 (1)
0 项奖励
回复
0 回复数