LPC1788 lcd controller configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 lcd controller configuration

4,890 次查看
atihaj
Contributor I

Hi 

I am new in arm cortex. The project I am working on it is developing LCD 3.5" with LPC1788.

Emwin library didn't work (stuck on GUI_init).

Then decided to setup on-chip lcd controller by my self. 

Now I have frequency 8MHZ on LCD_DCLK pin, but after power up, LCD_FP,LCD_LP ,LCD_LE and LCD_ENB all are low. only lcd_pwr is high. all LCD data(0..23) are low.

I would appreciate all advices.

Regards

Ati

0 项奖励
回复
1 回复

1,415 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Ati,

   I send you a LPC1788 LCD code for your reference, it is for the IAR LPC1788 board, I also attached the according schematic for your understanding.

  Please check the attachment.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复