LPC1788 is going crazy(No Exception) after calling SystemInit() function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 is going crazy(No Exception) after calling SystemInit() function

861件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cakmakmurat2000 on Wed May 23 09:41:09 MST 2012
Hi,

I have some LPC1788 ICs. One of them is on Embedded Artist Development Board and another ones are on my boards.
I call SystemInit() function on Embedded Artist Board and everything is OK. But When I try to call SystemInit() on Myboards, program counter jump meanless locations and do meanless something. There is no Exception (Hardfault, Busfault etc.)

If I dont call SystemInit() Embedded Artist and My Boards Behaviors are same.

Can it be Oscillator problem? I have changed Oscillator on my board but result is same.

Thanks.

Murat.
ラベル(1)
0 件の賞賛
返信
0 返答(返信)