LPC1788 USB Interfacing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 USB Interfacing

1,378件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jay123 on Mon May 19 23:19:02 MST 2014
Hello,

Microcontroller Use: LPC1788

presently i'm downloading my application through RS232 serial communication, but downloading time increase with increase in application size .
so  now i want to implement USB for fast download.

basic software requirement
a) USB initialize function
b) read function
c) write function

i have computer application for application download, in that application i select COM port, and other required setting after completion of setting  i hit download button and its start downloading, similarly i want same for USB, when i connect USB cable to computer it should generate USB device say USB0 and USB0 use for downloading.

please help me to implement USB Device
ラベル(1)
0 件の賞賛
返信
1 返信

1,313件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embd02161991 on Fri May 23 12:38:52 MST 2014
Hi,

You can try using the usb mass storage class example on lpcware.com and develop to implement your application.

http://www.lpcware.com/content/nxpfile/lpcopen-software-development-platform-lpc17xx-packages


Thanks

NXP Technical Support
0 件の賞賛
返信