LPC1788: USB D+ Line pull-down after 11us

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788: USB D+ Line pull-down after 11us

1,101 次查看
paul_shaffer
Contributor I

I would like more information about theUSB 2.0  D-PLUS line on the NXP part number LPC1788 microcontroller. When we power up, the D+ line starts to go "tri-state", then after 11us, the D+ line is internally pull-down to ground.  Why?

0 项奖励
回复
1 回复

1,076 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hi Paul,

In the LPC1788 the USB D+ is initially a GPIO pin, which after a reset is configured as an input. This will cause it to be at a high impedance. Once the usb is configured and the internal pull down is enabled you will see the change in state. However this behavior from its power on state to once the pins are configured should not impact your project.

If you have any further questions please dont hesitate to ask.

Hope this helps and have a great day!

Sabina

0 项奖励
回复