LPC1788, SSP1 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788, SSP1 problem

1,895件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MRF_PRL on Sat Nov 23 04:28:31 MST 2013

Hi dear all

I used a LPC1788 and I configured SSP1, but I can't write to LPC_SSP1 -> DR. I also configured SSP0, and it works very good and when I write LPC_SSP0 -> DR = 0xAA, its value will update, but for SSP1 it doesn't work.

Please Help me

Thanks
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,769件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Sun Nov 24 05:46:09 MST 2013
Hi,

from user manual:
SSP (base address 0x4008 8000 (SSP0), 0x4003 0000 (SSP1), 0x400A C000 (SSP2))

I assume your address SSP0 was a cut&paste error in the posting?
What happens when you write? Do you get into some fault handler (e.g. hard fault)?

What values do you write into CR0, CR1, CPSR to initialize the interface?

Have you seen chapter 21.1:

The three SSP interfaces, SSP0, SSP1, and SSP2 are configured using the following registers:
1. Power: In the PCONP register (Table 16), set bit PCSSP0 to enable SSP0 and bit PCSSP1 to enable SSP1.
Remark: On reset, SSP interfaces 0 and 1 are enabled (PCSSP0/1 = 1), while SSP2 is disabled (PCSSP2 = 0).
2. Peripheral clock: The SSPs operate from the common PCLK that clocks both the bus interface
and functional portion of most APB peripherals. See Section 3.3.21. In master mode, the clock must be scaled down (see Section 21.6.5).
3. Pins: Select the SSP pins and pin modes through the relevant IOCON registers (Section 7.4.1).
4. Interrupts: Interrupts are enabled in the SSP0IMSC register for SSP0 and SSP1IMSC register for SSP1 Table 482.
Interrupts are enabled in the NVIC using the appropriate Interrupt Set Enable register, see Table 48.
5. Initialization: There are two control registers for each of the SSP ports to be configured:
SSP0CR0 and SSP0CR1 for SSP0, SSP1CR0 and SSP1CR1 for SSP1,
SSP2CR0 and SSP2CR1 for SSP2. See Section 21.6.1 and Section 21.6.2.
6. DMA: The Rx and Tx FIFOs of the SSP interfaces can be connected to the GPDMA
controller (see Section 21.6.10). For GPDMA system connections, see Table 685.

Have you done at least steps 1, 2, 3 and 5? 4 only if you use interrupt, 6 if you use DMA.

Best regards,

Martin
0 件の賞賛
返信

1,769件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MRF_PRL on Sun Nov 24 05:23:40 MST 2013

Hi dear Martin

Thanks you for answering.
SSP1 data register mapped in 0x40030008, I want to write in this address, But I cant. For SSP0, data register mapped in 0x40080008, whenever SSP0 is activated, I can read and write this address, but for SSP1, also I active this peripheral, but I cant read and write, and this address only has 0x0000000 value :(.
I used Keil and though system_Lpc17xx, I active SSP1 :)

Thanks
0 件の賞賛
返信

1,769件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by capiman on Sat Nov 23 04:33:21 MST 2013
Hi,

sorry, details are not enough to give hints!

Can you please show some code which works and code which does not work?
Perhaps you have some code in use which still accesses SSP1 instead of SSP0?
How you powered up the correct peripheral?

Best regards,

Martin
0 件の賞賛
返信