LPC1788 SPI SCK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 SPI SCK

1,541件の閲覧回数
ljun_cdut
Contributor I

Recently,I am debugging the spi communitcation of LPC1788 . In master mode, how much is the max frequency of SPI ??

ラベル(1)
0 件の賞賛
返信
1 返信

1,331件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

The minimum clock cycle time, and therefore the maximum frequency of the SSP in master mode, is limited by the pin electronics to the value given. The SSP block should not be configured to generate a clock faster than that. At and below the maximum frequency, Tcy(clk) = (SSPCLKDIV  x  (1 + SCR) x CPSDVSR) / fmain. 5The clock cycle time derived from the SPI bit rate Tcy(clk) is a function of the main clock frequency fmain, the SSP peripheral clock divider (SSPCLKDIV), the SSP SCR parameter (specified in the SSP0CR0 register), and the SSP CPSDVSR parameter (specified in the SSP clock prescale register).


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信