LPC1788 SDRAM timing problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 SDRAM timing problem

3,209 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sebgonzo on Thu Jul 05 05:54:30 MST 2012
I'm making SDRAM layout for LPC1788. I want to do it right so I make timing budget calculations based on this article:

http://www.edn.com/design/test-and-measurement/4342433/Practical-timing-analysis-for-100-MHz-digital...

I think there are some errors in current datasheet (rev. 4 - May 2012) of LPC1788 (Table 18 on page 25):

th(Q) data output hold time   min. 0.2ns  max 1.6ns

If I understand it correctly this means, that data output is valid only for 0.2ns (worst case) after clock. My memory device, has minimum input hold time 0.8ns (and as I know most SDRAM's has similar value). Output hold time can't be lower than input hold time. I think this th(Q) is much to low.

I compared it with LPC1850 datasheet and in my opinion this is correct value (Table 23 on page 115):

th(Q) data output hold time   min. 0.5 × Tcy(clk) ns
where Tcy(clk) is clock period.

Also, I cant find any SDRAM layout guidelines for this microprocessor. I know there is Application Note for LPC32xx, but I can't find one for LPC1788.
标签 (1)
0 项奖励
回复
4 回复数

2,774 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sebgonzo on Fri Jul 06 07:40:50 MST 2012
Now everything it's clear. Thank you very much. It seems that I haven't read UM carefully.
0 项奖励
回复

2,774 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Fri Jul 06 06:51:39 MST 2012
sebgonzo,

there is more than ONE delay line!

- There is one delay line to adjust the delay between the SDRAM clock and all outgoing signals.
- And there is another delay line to adjust the delay between the SDRAM clock and the SDRAM read data latch.

You have to adjust both lines.
You may use from the following code fragments:


<code>
/* Transform ns into clock cycles (runtime, only 32bit multiplications):
* Valid input range: Clock < 995 MHz, ns = 0..1000000 (1ms)
*
* a) Divide Clock by 16. This gives enough headroom for step b).
* b) Multiply Clock by 69. This will adjust for decimal/binary divisor.
*    This computation will overflow for a clock > 995 MHz!
*    This computation will give results 0,5% larger than the real value.
* c) Divide Clock by 1048576 (2^20). This will give enough headroom for step d).
* d) Multiply Clock by ns. This will not overflow for ns = 0..1000000 (1ms).
* e) Divide Clock by 4096 (2^12). This will give value in clocks.
* f) Add 1 to account for rounding.
* (Use runtime computations because frequencies may change in runtime).
*/
#define NS_2_EMC_CLKS(ns) ((((((EMCClock >> 4)*69) >> 20)*(ns))>>12)+1)
#define NS_2_CPU_CLKS(ns) ((((((SystemCoreClock >> 4)*69) >> 20)*(ns))>>12)+1)

// Delay loop for short busy waits
__attribute__( ( always_inline ) ) static inline void wait_clocks( unsigned int clocks)
{
   clocks >>= 1;          // 2 Takte pro Durchlauf
   while(clocks--) {
      asm("":::"memory"); // hint for gcc: do not remove this loop!
   }
}

/*----------------------------------------------------------------------------
  MPU Defines
*----------------------------------------------------------------------------*/
#define SIZE_32B    0x04
#define SIZE_64B    0x05
#define SIZE_128B   0x06
#define SIZE_256B   0x07
#define SIZE_512B   0x08
#define SIZE_1K     0x09
#define SIZE_2K     0x0A
#define SIZE_4K     0x0B
#define SIZE_8K     0x0C
#define SIZE_16K    0x0D
#define SIZE_32K    0x0E
#define SIZE_64K    0x0F
#define SIZE_128K   0x10
#define SIZE_256K   0x11
#define SIZE_512K   0x12
#define SIZE_1M     0x13
#define SIZE_2M     0x14
#define SIZE_4M     0x15
#define SIZE_8M     0x16
#define SIZE_16M    0x17
#define SIZE_32M    0x18
#define SIZE_64M    0x19
#define SIZE_128M   0x1A
#define SIZE_256M   0x1B
#define SIZE_512M   0x1C
#define SIZE_1G     0x1D
#define SIZE_2G     0x1E
#define SIZE_4G     0x1F

#define AP_NONE     0x00
#define AP_RW       0x03

#define MEM_TYPE_STRONGLY 0x04          // Strongly ordered, Sharable, no Cache, no Buffer, no allocate
#define MEM_TYPE_FLASH    0x02          // Normal, Non-Sharable, Cached, no Buffer, write-through
#define MEM_TYPE_IRAM     0x06          // Normal, Sharable, Cached, no Buffer, write-through
#define MEM_TYPE_ERAM     0x07          // Normal, Sharable, Cached, Buffered, write-back & write allocate
#define MEM_TYPE_DEVICE   0x05          // Device, Sharable, no Cache, Buffered, no allocate

#define _RBAR(_ADDR, _VALID, _REGION) \
((_ADDR) | ((_VALID) << 4) | (_REGION))

#define _RASR(_XN, _AP, _TYPE, _SRD, _SIZE, _ENABLE) \
(((_XN) << 28) | ((_AP) << 24) | ((_TYPE) << 16) | ((_SRD) << 8) | ((_SIZE) << 1) | (_ENABLE))

/*----------------------------------------------------------------------------
  SDRAM calculation values
*----------------------------------------------------------------------------*/
// Timing for a 133 MHz SDRAM (-75), calculated in clocks
#define RAS_LATENCY NS_2_EMC_CLKS(20)
#define CAS_LATENCY 2
#define T_RP        NS_2_EMC_CLKS(20)
#define T_RAS       NS_2_EMC_CLKS(45)
#define T_SREX      NS_2_EMC_CLKS(72)
#define T_APR       NS_2_EMC_CLKS(20)
#define T_DAL       (CAS_LATENCY+2)
#define T_WR        2
#define T_RC        NS_2_EMC_CLKS(65)
#define T_RFC       NS_2_EMC_CLKS(75)
#define T_XSR       NS_2_EMC_CLKS(72)
#define T_RRD       NS_2_EMC_CLKS(15)
#define T_MRD       2
#define T_REFRESH   NS_2_EMC_CLKS(15625)

// Default Delays. Quelle: praktische Versuche
// mit dem Embedded Artist Board . EMC Clock <= 80MHz, Command Delay Strategie +0.
#define DEFAULT_CLKOUTDLY 0
#define DEFAULT_FBCLKDLY  20
#define DEFAULT_CMDDLY    16

/**
* SDRAM Delay line calibration.
* The estimated value gives a hint to correct the SDRAM timings.
* @param  none
* @return value 0..4095 corresponding to the speed of logic.
*         Faster logik (less delay) gives larger output values.
*/
static unsigned int Calibrate (void)
{
   unsigned int i;
   unsigned int value = 0;
   unsigned int data;

   for (i = 16; i; i--) {        // get a mean value
      LPC_SC->EMCCAL = 0x4000;   // start calibration
      do {
         data = LPC_SC->EMCCAL;
      } while (!(data & 0x8000));// wait until DONE
      value += data & 0xFF;
   }
   return value;
}

/**
* SDRAM Test.
* This is used at startup time (before the first usage) to find the optimum
* delay time values.
* ATT: This test overwrites the previous SDRAM contents!
* Please note that IT IS NOT POSSIBLE to preserve these contents because
* it might be possible that garbage address commands are output and we will
* not know which locations are addressed during this test.
* DO NOT USE this test if executing code from SDRAM.
* @param       offsetKonstante, um das Testpattern zu modifizieren
* @return      1 if test OK, 0 if failure
* */
static int sdram_check(uint32_t offset)
{
  volatile uint32_t *ram_ptr;
  uint32_t data;
  uint32_t i,j;
  uint32_t blocks;
#define SDRAMTEST_BLOCKSIZE 0x100
#define SDRAMTEST_JUMPSIZE  0x10000

  blocks = SDRAM_SIZE/(sizeof(uint32_t) * SDRAMTEST_JUMPSIZE);

  /* writing */
  ram_ptr = (uint32_t *)SDRAM_START;
  data = 0x10000 + offset;
  for (i = 0; i < blocks; i++)
  {
    for (j = 0; j < SDRAMTEST_BLOCKSIZE; j++)
    {
       *ram_ptr++ = data;
       data += j + (j << 4);
    }
    ram_ptr += SDRAMTEST_JUMPSIZE - SDRAMTEST_BLOCKSIZE;
    data += i + (i << 4);
  }

  /* Verifying */
  ram_ptr = (uint32_t *)SDRAM_START;
  data = 0x10000 + offset;
  for (i = 0; i < blocks; i++)
  {
    for (j = 0; j < SDRAMTEST_BLOCKSIZE; j++)
    {
       if (data != *ram_ptr++)
          return 0;
       data += j + (j << 4);
    }
    ram_ptr += SDRAMTEST_JUMPSIZE - SDRAMTEST_BLOCKSIZE;
    data += i + (i << 4);
  }
  return 1;
}

/**
* Optimize the SDRAM delays.
* The complete range of a delay (0..31) is set, then tested by a SDRAM test.
* Output value is the middle of the functional range.
* @param shift     Bitshift value to point to the delay position in EMCDLYCTL
* @param def_value  Value to set if no positive range can be found.
* @return           Optimum value which is set in EMCDLYCTL.
*/
static unsigned int Optimize_Delay( unsigned int shift, unsigned int def_value)
{
   int i;
   int start_delay = -1;
   int stop_delay = -1;
#define DELAY_RANGE 0x1F

   for (i = 0; i <= DELAY_RANGE; i++) {
      // set delay value
      LPC_SC->EMCDLYCTL = ( LPC_SC->EMCDLYCTL & ~(DELAY_RANGE << shift) ) | (i << shift) ;
      if (sdram_check(i+10+shift)) {
         if (start_delay < 0)
            start_delay = i;
         stop_delay = i;
      }
   }
   // Hier an dieser Stelle wissen wir, ob das SDRAM ueberhaupt vernuenftig geht.
   if ((stop_delay - start_delay) < 3) {
       // Tja, damit kann man kein Telefon fahren
       while (1)
           {};
   }
 
   i = (start_delay + stop_delay) / 2;
   if (i < 0)
      i = def_value;
   // set new delay value
   LPC_SC->EMCDLYCTL = ( LPC_SC->EMCDLYCTL & ~(DELAY_RANGE << shift) ) | (i << shift);
   return i;
}



  // configure the dynamic memory read strategy.
  // ------------------------------------------------------------------------------------------
  LPC_EMC->DynamicReadConfig = 0x00000001;  // Command delayed strategy + 0, using EMCCLKDELAY
                                            // (command delayed, clock out not delayed)
  /* Anmerkung:
   * mit Clockout Delayed Strategie (00) kann man die Data Hold Time (NXP min 0,2ns, SDRAM min 1,0ns)
   * nicht mehr sicher erreichen, also muss man zwangsweise Command Delayed verwenden.
   */



   // Default-Werte fuer Delaylines setzen
   LPC_SC->EMCDLYCTL = (DEFAULT_CLKOUTDLY << 24) | (DEFAULT_CLKOUTDLY << 16) | (DEFAULT_FBCLKDLY << 8) | DEFAULT_CMDDLY;



  // do the reference calibration
  perm.initial_calibration_value = Calibrate();


     // Delay-startwerte ausmessen, setzen und aufbewahren
     perm.original_cmdclkdelay = Optimize_Delay( 0, DEFAULT_CMDDLY);
     perm.original_fbclkdelay  = Optimize_Delay( 8, DEFAULT_FBCLKDLY);


     // wir sind im Bootloader
     MPU->CTRL = 0x00;             // MPU disablen

     // Flush into MPU
     __ISB();                      // instruction memory barrier

     // Die Regionen sind mit unterschiedlicher Prioritaet versehen. Region 0 ist
     // die unterste, d.h. man kann sie gut als Default verwenden. Und wenn man sie so
     // programmiert, dass alle Zugriffe verboten sind, so kann man damit ungueltige
     // Speicherzugriffe abfangen und die Software neu starten.

     // Region 0: Default ohne Zugriffsrechte, gesamter Adressbereich
     MPU->RBAR = _RBAR(0x00000000, 1, 0);
     MPU->RASR = _RASR(1, AP_NONE, MEM_TYPE_STRONGLY, 0, SIZE_4G, 1);

     // Region 1: internes Flash, internes SRAM, Boot ROM,
     //           Peripheral SRAM, AHB Peripherals
     // 0x00000000 - 0x3FFFFFFF
     // Subregions: 0 = Flash, 2 = SRAM, 3 = Boot ROM,
     //             4 = Peripheral SRAM + AHB Peripherals
     MPU->RBAR = _RBAR(0x00000000, 1, 1);
     MPU->RASR = _RASR(0, AP_RW, MEM_TYPE_IRAM, 0xE2, SIZE_1G, 1);

     // Region 2: Peripheral Devices
     // 0x40000000 - 0x400FFFFF
     // 0x42000000 - 0x43FFFFFF Bitband-Alias
     MPU->RBAR = _RBAR(0x40000000, 1, 2);
     MPU->RASR = _RASR(1, AP_RW, MEM_TYPE_DEVICE, 0, SIZE_64M, 1);

     // Region 3: ext. Chip Selects/Devices (XHFC)
     // 0x80000000 - 0x9000FFFF
     MPU->RBAR = _RBAR(0x80000000, 1, 3);
     MPU->RASR = _RASR(1, AP_RW, MEM_TYPE_DEVICE, 0, SIZE_64K, 1);

     // Region 4: SDRAM
     // 0xA0000000 - 0xA0FFFFFF
     MPU->RBAR = _RBAR(0xA0000000, 1, 4);
     MPU->RASR = _RASR(0, AP_RW, MEM_TYPE_ERAM, 0, SIZE_16M, 1);

     // Region 5: Cortex-M3 Private Peripheral Bus
     // 0xE0000000 - 0xE00FFFFF
     MPU->RBAR = _RBAR(0xE0000000, 1, 5);
     MPU->RASR = _RASR(1, AP_RW, MEM_TYPE_STRONGLY, 0, SIZE_1M, 1);

     // Region 6: not used (immer gut, eine frei zu haben)
     MPU->RBAR = _RBAR(0x00000000, 1, 6);
     MPU->RASR = _RASR(0, 0, 0, 0, 0, 0);

     // Region 7: Stack check
     MPU->RBAR = _RBAR(STACK_START, 1, 7);
     MPU->RASR = _RASR(1, AP_NONE, MEM_TYPE_IRAM, 0, SIZE_32B, 1);

     // MPU (wieder) einschalten
     MPU->CTRL = 0x01;       // MPU enabled

  }
  // Flush into MPU
  __DSB();                 // Data Sync
  __ISB();                // instruction memory barrier





/** Diese Routine sollte in regelmaessigen Abstaenden aufgerufen werden,
* um das Timing bei Aenderungen der Umgebungsbedingungen abzustimmen.
*/
void adjust_timing (void)
{
   // wie schnell sind wir denn heute?
   unsigned int calibration_value = Calibrate();

   // neue Kalibrierwerte errechnen
   unsigned int fbclkdelay  = ((perm.original_fbclkdelay  * calibration_value) / perm.initial_calibration_value);
   unsigned int cmdclkdelay = ((perm.original_cmdclkdelay * calibration_value) / perm.initial_calibration_value);

   // Check the range, luke
   if (fbclkdelay > 0x1F)
      fbclkdelay = 0x1F;
   if (cmdclkdelay > 0x1F)
      cmdclkdelay = 0x1F;

   // Set new values
   LPC_SC->EMCDLYCTL = (DEFAULT_CLKOUTDLY << 24) | (DEFAULT_CLKOUTDLY << 16)
                     | (fbclkdelay << 8) | cmdclkdelay;
}


0 项奖励
回复

2,774 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by sebgonzo on Fri Jul 06 05:11:13 MST 2012
Yes, I understand what for delay lines are. You can introduce delay to the controller clock, to compensate sdram clock delay. I'm sure that your solution is ok, but I want to do some calculations, because I'm doing PCB layout now and I want do know if it's ok. But the problem is that with timing parameters from datasheet sdram will not work, so this is why I'm suggesting an error in dataheet (or maybe I'm doing something wrong).

Here is my calculations:
Tclk = 12.5ns (clock period for 80MHz clock)
TOF = 0.67ns (time of flight for 50mm data traces)
Tskew = 0ns (skew between controller clock and SDRAM clock)

Write operation (Controller to SDRAM)
toh(CTRL)min = 0.2ns (controller minimum output data hold time)
td(CTRL)max = 8.7ns (controlle maximum clock to data valid output delay)
tsu(SDRAM)min = 1.5ns (SDRAM minimum setup time)
th(SDRAM)min = 0.8ns (SDRAM minimum hold time)

setup margin = Tclk - td(CTRL)max - TOF + Tskew - tsu(SDRAM)min = 12.5 - 8.7 - 0.67 - 0 - 1.5 = 1.63ns
hold margin = toh(CTRL)min + TOF - th(SDRAM)min - Tskew = 0.2 + 0.67 - 0.8 - 0 = 0.07ns

Setup margin is ok, but hold margin is too low so let's introduce some clock skew.

Tskew = -0.5ns
setup margin = 12.5 - 8.7 - 0.67 + (-0.5) - 1.5 = 1.13ns
hold margin = 0.2 + 0.67 - 0.8 - (-0.5) = 0.57ns

Now it's quite ok but let's look at Read operation (SDRAM to Controler)
toh(SDRAM)min = 1.8ns (SDRAM minimum output data hold time)
td(SDRAM)max = 6ns (SDRAM maximum clock to data valid output delay - access time)
tsu(CTRL)min = 1.5ns (controller minimum setup time)
th(CTRL)min = 3.7ns (controller minimum hold time)

Tskew = 0.5ns (becuase we changed data direction - SDRAM is transmitting, controller is receiving)

setup margin = 12.5 - 6 - 0.67 + 0.5 - 1.5 = 4.83ns
hold margin = 1.8 + 0.67 - 3.7 - 0.5 = -1.73ns

Hold time is negative so our SDRAM is not working at all. I can't find Tskew that both read and write time requirements are ok.

I know that my post is a bit complicated, but I'd like that someone verify my calculations (the best is someone from NXP) and say that I'm wrong or there is an error in datasheet.
0 项奖励
回复

2,774 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Thu Jul 05 07:54:49 MST 2012
Are you sure you have read and understand the purpose of the delay lines in the SDRAM controller?

Please refer to the manual on the ARM website!

In order to use the SDRAM with LPC17xx, you have to
- setup the SDRAM controller, using default values for the delay lines.
- Doing a RAM test, checking the minimum and maximum usable delays.
- store the selected delays (== the "original" values).
- measure the special delay line for compensation == original reference value)

Inside your application,
- measure the special delay line.
- Adjust the other delay lines according to the original values * (actual / reference).

Ugly but working.

0 项奖励
回复