LPC1788 RTC backup registers data missing randomly, Although Vbat is available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 RTC backup registers data missing randomly, Although Vbat is available

1,913 次查看
PMGJ1
Contributor I

Hi,

We are using the LPC1788 controller in our applications.

If the power goes out to the controller, we need to hold some information.

For that we are using GPREG0,1 and 2 registers to save the data. We are also using RTC with Vbat(3.2V Coin cell).

But, even if the RTC works well after the power outage, the data stored in the registers is missed sometimes. This issue is occurring randomly.

 

标签 (1)
0 项奖励
回复
2 回复数

1,809 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @PMGJ1 

 

Thank you so much for reaching us in our community. I would like to apologize for the delay, but we are experimenting a high volume of questions these days. I really appreciate your patience.

 

I would like to help you, so may I know if it is possible, are you using your custom board with LPC1788 or you are using a development board from NXP ? So I can reproduce your issue on our boards and see what is going on, it is too weird that occurs randomly, it comes to my mind that it is a HW issue.

 

I will stay tuned to your reply, so I can help you further. Please let me know if you have more questions.

 

Sincerely,
Pablo Avalos.

0 项奖励
回复

1,847 次查看
PMGJ1
Contributor I

Any update on the above problem. Please suggest!!!

0 项奖励
回复