LPC1788 & NXP-emWin538-libraries, compile error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 & NXP-emWin538-libraries, compile error

2,421 Views
myz
Contributor I
Hello , All:
        I am used LPC1788 & emwin5.30c in my new product .But I find a bug in emwin5.30c, so I want update emwin to 5.38 version. My compiler is keil mdk 5.23,  I download NXP-emWin538-libraries.zip and replace emwin5.30c in my project .The compile Error like this:
.\Objects\DispPrj.axf: Error: L6366E: WM_ValidateWindow.o attributes are not compatible with the provided attributes .
Object WM_ValidateWindow.o contains Build Attributes that are incompatible with the provided attributes.
    Tag_CPU_arch = ARM v7E-M (=13)
.\Objects\DispPrj.axf: Error: L6366E: WM__ForEachDesc.o attributes are not compatible with the provided attributes .
Object WM__ForEachDesc.o contains Build Attributes that are incompatible with the provided attributes.
    Tag_CPU_arch = ARM v7E-M (=13)
        Error nums up to 239. I don't know what occurred , and how can I sovle these errors?
        Thanks and wait for help.
Labels (2)
0 Kudos
Reply
3 Replies

2,017 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi my z,

    Did you add the according lib path in the IDE?

    You can send me your test project, I will help you to check it on my side.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,017 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi my z,

   I have reproduced your problem on my side.

  I think it should be the new lib problem, please use the emwin5.30c now, I will check the new emwin problem with our according department.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,017 Views
myz
Contributor I

Hi Kerry:

I found some bugs from emwin5.30c,older emwin version can not support truetype(I tested,seem), Can I use 5.32 or 5.36?Where I can download these version? And when will correct 5.38?

Thank you

0 Kudos
Reply