LPC1788 - External SDRAM connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 - External SDRAM connection

1,307 次查看
lorenzogalbiati
Contributor I

Hello,

I've never used external SDRAM with LPC1788 controller and I have some doubts about connection. I'm developing a commercial product for my factory so I need to be sure about that.

I have chosen IS42S16100H (512K Words x 16 Bits x 2 Banks) and I wonder if it is supported by LPC1788. Mapping table reports 16Mbit (1Mx16), 2 banks. Is this the same configuration?

2024-08-09_132742.jpg

The second question is about address bus: this SDRAM has A0-A10 and A11 for bank select.

I have connected to EMC_A[0]...EMC_A[11]. Is this correct? Should A11 be connected in a different way because it's a bank selector???

2024-08-09_133154.jpg

 

Many thanks for every help. I need assistance.

Greetings

 

 

标签 (1)
0 项奖励
回复
1 回复

1,273 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The IS42S16100H has 8 column  address, 11 row address, so you can select the address configuration as the yellow color.

Because there is only one bank, you have to connect the A11 of SDRAM to EMC_A[13].

Hope it can help you

BR

Xiangjun Rong

 

xiangjun_rong_0-1723531837098.png

 

0 项奖励
回复