LPC1788 - External SDRAM connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1788 - External SDRAM connection

1,233件の閲覧回数
lorenzogalbiati
Contributor I

Hello,

I've never used external SDRAM with LPC1788 controller and I have some doubts about connection. I'm developing a commercial product for my factory so I need to be sure about that.

I have chosen IS42S16100H (512K Words x 16 Bits x 2 Banks) and I wonder if it is supported by LPC1788. Mapping table reports 16Mbit (1Mx16), 2 banks. Is this the same configuration?

2024-08-09_132742.jpg2024-08-09_132742.jpg

The second question is about address bus: this SDRAM has A0-A10 and A11 for bank select.

I have connected to EMC_A[0]...EMC_A[11]. Is this correct? Should A11 be connected in a different way because it's a bank selector???

2024-08-09_133154.jpg2024-08-09_133154.jpg

 

Many thanks for every help. I need assistance.

Greetings

 

 

ラベル(1)
0 件の賞賛
返信
1 返信

1,199件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The IS42S16100H has 8 column  address, 11 row address, so you can select the address configuration as the yellow color.

Because there is only one bank, you have to connect the A11 of SDRAM to EMC_A[13].

Hope it can help you

BR

Xiangjun Rong

 

xiangjun_rong_0-1723531837098.pngxiangjun_rong_0-1723531837098.png

 

0 件の賞賛
返信