LPC1788 - External SDRAM connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 - External SDRAM connection

1,359 Views
lorenzogalbiati
Contributor I

Hello,

I've never used external SDRAM with LPC1788 controller and I have some doubts about connection. I'm developing a commercial product for my factory so I need to be sure about that.

I have chosen IS42S16100H (512K Words x 16 Bits x 2 Banks) and I wonder if it is supported by LPC1788. Mapping table reports 16Mbit (1Mx16), 2 banks. Is this the same configuration?

2024-08-09_132742.jpg

The second question is about address bus: this SDRAM has A0-A10 and A11 for bank select.

I have connected to EMC_A[0]...EMC_A[11]. Is this correct? Should A11 be connected in a different way because it's a bank selector???

2024-08-09_133154.jpg

 

Many thanks for every help. I need assistance.

Greetings

 

 

Labels (1)
0 Kudos
Reply
1 Reply

1,325 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The IS42S16100H has 8 column  address, 11 row address, so you can select the address configuration as the yellow color.

Because there is only one bank, you have to connect the A11 of SDRAM to EMC_A[13].

Hope it can help you

BR

Xiangjun Rong

 

xiangjun_rong_0-1723531837098.png

 

0 Kudos
Reply