LPC1788 8bpp LCD Interface connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1788 8bpp LCD Interface connection

1,716 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jay123 on Mon Jul 20 23:28:54 MST 2015
i'm using graphic LCD with 24 color lines (8xR+8xB+8xG). i want to connect lcd with LPC1788 in 8bpp 332 mode.

anybody know connnection diagram in 332 and 323 mode?

if i configured segger for 16bit 565 color conversion mode then it takes more time to update LCD then 8 bit LCD driver.
update time of 8bit is 80% faster than 16bit so i want to interface LCD in 8bit 332 (RGB mode) only.

Segger configuration:
16 bit configuration:
#define COLOR_CONVERSION   GUICC_565
#define DISPLAY_DRIVER     GUIDRV_LIN_16

8 bit configuration:
#define COLOR_CONVERSION   GUICC_332
#define DISPLAY_DRIVER     GUIDRV_LIN_8

Result:
Sr No | Segger config | LCD Config | Conclusion
1        | 16bpp            |  16 bpp       | display properly but update time is too slow
2        | 8bpp              |  16 bpp       | not display proper shown in attach image (8bpp) but update time is better
3        | 8bpp              |  8 bpp         | display blank only backlight turns ON

attach image :
A,b -> display two times
c --> display junk data

in 2nd case image is drawn twice and scale by 4 but it should display as shown in attach image(expected).

which pins are use for 8bit 332 RGB mode???
please share schematic of same
Labels (1)
0 Kudos
Reply
1 Reply

1,619 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by jay123 on Tue Jul 21 22:58:41 MST 2015
NXP please provide solution.

pin assignment missing in usermanual..
0 Kudos
Reply