LPC1785 and SDRAM issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1785 and SDRAM issue

1,621 Views
giusloq
Contributor III

I designed a custom 4-layers PCB with LPC1785 (208 pins) and SDRAM (MT48LC2M32B2, 512K x 32 x 4 Banks from Micron). The connections are the same as in EA 1788 dev board:

  • EMC_A[0:11] to A[11:0] of SDRAM
  • EMC_A12 not connected
  • EMC_A13 to BA0; EMC_A14 to BA1
  • EMC_D[31:0] to D[31:0] of SDRAM
  • EMC_DQM[3:0] to DQM[3:0] of SDRAM
  • EMC_CLK0 to CLK of SDRAM; EMC_CKE0 to CKE of SDRAM
  • EMC_CLK1 and EMC_CKE[3:1] not connected
  • EMC_WE, EMC_CAS, EMC_RAS to WE, CAS, RAS of SDRAM
  • EMC_DYCS0 to CS of SDRAM
  • EMC_DYCS[3:1] not connected

I started from the example periph_memtest found in LPCOpen v2.10. I only changed the function Board_SetupClocking() to avoid SPIFI clock configuration and to call Chip_SetupIrcClocking() instead of Chip_SetupXtalClocking() (actually the crystal isn't mounted on my board).

void Board_SetupClocking(void)
{
/* Enable PBOOST for CPU clock over 100MHz */
Chip_SYSCTL_EnableBoost();

//Chip_SetupXtalClocking();
Chip_SetupIrcClocking();

/* SPIFI clocking will be derived from Main PLL with a divider of 2 (60MHz) */
//Chip_Clock_SetSPIFIClockDiv(2);
//Chip_Clock_SetSPIFIClockSource(SYSCTL_SPIFICLKSRC_MAINPLL);

}

I also changed Board_SetupExtMemory() function commenting static memories configuration.

/* Setup external memories */
void Board_SetupExtMemory(void)
{
   /* Setup EMC Delays */
   /* Move all clock delays together */
   LPC_SYSCTL->EMCDLYCTL = (CLK0_DELAY) | (CLK0_DELAY << 8) | (CLK0_DELAY << 16 | (CLK0_DELAY << 24));

   /* Setup EMC Clock Divider for divide by 2 */
   /* Setup EMC clock for a divider of 2 from CPU clock. Enable EMC clock for
external memory setup of DRAM. */
   Chip_Clock_SetEMCClockDiv(SYSCTL_EMC_DIV2);
   Chip_SYSCTL_PeriphReset(SYSCTL_RESET_EMC);

   /* Init EMC Controller -Enable-LE mode- clock ratio 1:1 */
   Chip_EMC_Init(1, 0, 0);

   /* Init EMC Dynamic Controller */
   Chip_EMC_Dynamic_Init((IP_EMC_DYN_CONFIG_T *) &IS42S32800D_config);

   /* Init EMC Static Controller CS0 */
   //Chip_EMC_Static_Init((IP_EMC_STATIC_CONFIG_T *) &SST39VF320_config);

   /* Init EMC Static Controller CS1 */
   //Chip_EMC_Static_Init((IP_EMC_STATIC_CONFIG_T *) &K9F1G_config);

   /* EMC Shift Control */
   LPC_SYSCTL->SCS |= 1;
}

I also changed the configuration structure of SDRAM to reflect the real memory configuration (512k x 32 x 4 banks):

STATIC const IP_EMC_DYN_CONFIG_T IS42S32800D_config = {
   EMC_NANOSECOND(64000000 / 4096),
   0x01, /* Command Delayed */
   3, /* tRP */
   7, /* tRAS */
   EMC_NANOSECOND(70), /* tSREX */
   EMC_CLOCK(0x01), /* tAPR */
   EMC_CLOCK(0x05), /* tDAL */
   EMC_NANOSECOND(12), /* tWR */
   EMC_NANOSECOND(60), /* tRC */
   EMC_NANOSECOND(60), /* tRFC */
   EMC_NANOSECOND(70), /* tXSR */
   EMC_NANOSECOND(12), /* tRRD */
   EMC_CLOCK(0x02), /* tMRD */
   {
      {
         EMC_ADDRESS_DYCS0, /* EA Board uses DYCS0 for SDRAM */
         2, /* RAS */

         EMC_DYN_MODE_WBMODE_PROGRAMMED |
         EMC_DYN_MODE_OPMODE_STANDARD |
         EMC_DYN_MODE_CAS_2
         EMC_DYN_MODE_BURST_TYPE_SEQUENTIAL |
         EMC_DYN_MODE_BURST_LEN_4,

         EMC_DYN_CONFIG_DATA_BUS_32 |
         EMC_DYN_CONFIG_LPSDRAM |
         EMC_DYN_CONFIG_2Mx32_4BANKS_11ROWS_8COLS | //EMC_DYN_CONFIG_8Mx16_4BANKS_12ROWS_9COLS |
         EMC_DYN_CONFIG_MD_SDRAM
      },
      {0, 0, 0, 0},
      {0, 0, 0, 0},
      {0, 0, 0, 0}
   }
};

Labels (2)
Tags (4)
0 Kudos
Reply
1 Reply

1,430 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Giuseppe Modugno,

Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
I'm working on it, and I was wondering if you can tell me what the kind of issue happens.
Have a great day,

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply