LPC1785 CRP2 Upgrade Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1785 CRP2 Upgrade Problem

831件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Arnold.K on Tue Jan 29 18:37:03 MST 2013
Dear ALL,

I have two problems regarding upgrade the LPC 1785 after using the Level 2 Code Read Protection.

First, as CRP2 need to use the JTAG. I may want to ask can I use IAP to upgrade my code by UART? How can I do this? Also, is that we need to use P0(2) and P0(3).

Second, with the CRP2, can I use SD card to upgrade? If yes, how?

Thank you so much.

Best Regards
Arnold
Fustec
ラベル(1)
0 件の賞賛
返信
0 返答(返信)