LPC177x_8x Pin Mux tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC177x_8x Pin Mux tool

1,207 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sun Oct 21 23:56:46 MST 2012
In the files section for 177x/8x there is "LPC177x_8x Pin Mux tool".

This zip appears to contain a jar file.

How is this run?

If I double click in WinZip, it tells me that the system is not
configured to view the file.

Any help would be appreciated.
Labels (1)
0 Kudos
Reply
3 Replies

1,183 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexan.e on Mon Nov 05 01:47:50 MST 2012
Yes you are right it works fine.

I originally thought you were asking for lpc expert which is a different tool http://www.lpcware.com/blogs/lpcxpert.
There is a pin mux mentioned in that title of that application so I thought you were referring to it.

Alex
0 Kudos
Reply

1,183 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SebLo on Mon Nov 05 00:38:01 MST 2012

It work fine, I work with windows 7 and I open it with "Java(TM) Platform SE binary"
0 Kudos
Reply

1,183 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by alexan.e on Mon Oct 22 03:16:53 MST 2012
Hi

It is a java based application, I tried to use it a while ago but I had some problems in windows XP.

You can try a similar free application which is a windows executable and can run both in windows or linux (using WINE) http://alexan.edaboard.eu/

Alex
0 Kudos
Reply