LPC177X JTAG Connection Problem - Confusion on pull-ups, pull-downs on JTAG pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC177X JTAG Connection Problem - Confusion on pull-ups, pull-downs on JTAG pins

1,172件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cem.ayyildiz on Tue Dec 02 02:56:14 MST 2014
I think, there is a confusion on pull-up, pull down resistors connected to JTAG interface of LPC177X.
In http://www.lpcware.com/content/faq/lpcxpresso/debug-design states that TCK pin should be connected to pull-down. In UM10470, it is connected to pull-up resistor.
Which one is correct?
ラベル(1)
0 件の賞賛
返信
1 返信

1,159件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Tue Dec 02 03:13:42 MST 2014
This was asked recently (and answered). You didn't look very hard did you.

See here.

Regards, Mike
0 件の賞賛
返信