LPC1778FBD208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778FBD208

4,677 Views
yukinobuhori
Contributor II

Help me. I received a request to write the source code to the target device. I received the board, schematic, and source code (hex). 1. LPC1788FBD208 is mounted on the board. 2. From which line do you write? 2-1. Signal name UART0_TX, UART0_RX USB connector--CP2102-GM (device)--LPC1788-20 2pin204pin 2-2. Signal name UART1_TX, UART1_RX Ethernet connector--LPC1788-128pin 130pin 2-3. Signal name UART2_TX, UART2_RX 5PIN connector--ADM232AARNZ (device)--LPC1788-98pin 100pin 2-4. Signal name JTAG 20PIN connector--LPC1788-20 6pin2pin4pin6pin8pin10pin 3. Source code (hex) is only one file 4. Purchase the necessary tools. teach me please. 5. Do you use Flash Magic tools or something? I have one more question. What is the difference between LPC1788FBD208 and LPC1778FBD208?

0 Kudos
Reply
4 Replies

4,637 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

 

Hello yukinobuhori,

1) About your first questions, could you please describe again, sorry don't understand very well .

2) "What is the difference between LPC1788FBD208 and LPC1778FBD208?"

>>  LPC1788FBD208 includes LCD, while  LPC1778FBD208 doesn't .

 

Alice_Yang_0-1633942794421.pngAlice_Yang_0-1633942794421.png

 

BR

Alice

0 Kudos
Reply

4,627 Views
yukinobuhori
Contributor II

I'm poor at the explanation and sorry. A circuit diagram is attached to reference.

A writing in request of source cord was received from a target device.
A substrate, a circuit diagram and source cord (hex) are kept for a customer.

1. LPC1788FBD208 is mounted on a substrate.

2. I have 4 of Rhein it seems possible to write in. From which line?
Is a source file (hex) written in?
Or, a necessary tool is bought. Please tell me.

2-1. Signal name UART0_TX,UART0_RX
USB-B connector--CP2102-GM (IC),--LPC1788-202pin204pin
2-2. Signal name UART1_TX,UART1_RX
Ethernet connector--LPC1788-128pin130pin
2-3. Signal name UART2_TX,UART2_RX
5PIN connector--ADM232AARNZ (IC),--LPC1788-98pin100pin
2-4. Signal name JTD0,JTD1,JTMS,JTRST,JTCK
20PIN connector--LPC1788-206pin2pin4pin6pin8pin10pin
3. Source cord (hex), only 1 file.
4. Flash Magic tool used?

0 Kudos
Reply

4,616 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello yukinobuhori,

Do you meaning you need write software code for the the board you attached?

If yes, you can use MCUXpresso IDE with LPCopen driver to development, also there is

demo under LPCopen you can refer to.

MCUXpresso IDE:

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-i...  

LPCopen for lpc1788:

https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcop...  

 

 

0 Kudos
Reply

4,601 Views
yukinobuhori
Contributor II

Thank you.
I will proceed with reference.

0 Kudos
Reply