LPC1778 unable to use P5_3 as an output

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1778 unable to use P5_3 as an output

1,080 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gvd@mgb-tech.com on Fri Dec 18 02:33:47 MST 2015
Hello,

It seems to be impossible to use pin P5_3 as an output.
Although I haven't found anything in the datasheet/user manual that confirms this.

This Pin is of the special I type and linked to the I2C functionality but it can be configured as a standard GPIO pin.
The I type pins can not select the GPIO mode setting (pull-up, pull-down, ...) but I assumed it could be used as a standard output pin.
Which seems to be impossible.

Anyone who has an explanation?
Or am I still missing something.

Gerrit
标签 (1)
0 项奖励
回复
3 回复数

1,069 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gvd@mgb-tech.com on Fri Dec 18 09:53:31 MST 2015
Sorry duplicate entry
0 项奖励
回复

1,069 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by gvd@mgb-tech.com on Fri Dec 18 09:28:04 MST 2015
Indeed

Thanks Serge

I'll go home and weep for the weekend
0 项奖励
回复

1,069 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by serge on Fri Dec 18 08:09:12 MST 2015
The datasheet tells us that P5_3 is an open drain..... forgot the external pullup?
0 项奖励
回复