LPC1778 bootloader issues

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1778 bootloader issues

2,140 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wiggerssander on Wed Jan 02 03:48:00 MST 2013
Hello,

I'm trying to make a custom bootloader for my lpc1778 (rev E).
This bootloader will be uploaded using the NXP bootloader and then run from internal ram.

So far I got the bootloader to be uploaded and running from ram. The main program reads the part ID using the IAP commands. If the part is a lpc1778 then a led will be turned on.

Now I want to setup the pll's to run the program from external crystal on 120MHz. Therefore I need to set the CPU clock divider (CCLKSEL register) to 1.

Although I think that I follow the correct procedure to (dis)connect and setup the pll's this doesn't work for this setting. But if I set the CPU clock divider to 2 (60MHz) it works just fine.

Can somebody help me please!?
My code is shown below..

Kind regards,
Sander

Code:

/*************************** FUNCTION ************************************/
sint32 main(void)
/*************************** INFO ***************************************
**
** DESCRIPTION : Main Program Flash OS.
**
**               Read and process Flash OS command (received from uart).
**
** INPUT       :
**
** OUTPUT      :
**
** RETURN      :
**************************************************************************/

  IAP iap_entry;

  uint32 command[5] = {0, 0, 0, 0, 0};
  uint32 output[5]  = {0, 0, 0, 0, 0};

  init_lpc_system();

  init_io();
  set_led(OUTP_RED_LED, TRUE);
 
  iap_entry = (IAP)0x1FFF1FF1;
 
  command[0] = 54;
  iap_entry((uint32 *)command, (uint32 *)output);
 
  if((output[0] == 0        )&&
     (output[1] == 655966023)  )
  {
    set_led(OUTP_GREEN_LED, TRUE);
  }
  else
    set_led(OUTP_GREEN_LED, FALSE);

  while(TRUE);
}

/*************************** FUNCTION ************************************/
void init_lpc_system(void)
/*************************** INFO ****************************************
**
** DESCRIPTION : Initialise the cortex-m3 core, and clocks.
**
** INPUT       : none
**
** OUTPUT      : none
**
** RETURN      : none
**************************************************************************/
{
  /**************************** DISABLE ALL PLL'S ************************/
  sc->pboost    = 0x00000003;
  sc->flashcfg = FLASHCFG_REG_VAL;
 
  sc->clksrcsel = CLKSRCSEL_REG_VAL;    // set pll 0 clock source
 
  sc->cclksel     = 0x00000001;
  sc->usbclksel   = 0x00000000;
  sc->spificlksel = 0x00000000;
 
  sc->pll0con   = 0x00;                 // disable pll 0
  sc->pll0feed  = 0xAA;
  sc->pll0feed  = 0x55;
 
  sc->pll1con   = 0x00;                 // disable pll 1
  sc->pll1feed  = 0xAA;
  sc->pll1feed  = 0x55;
 
  /**************************** MAIN CLOCK *******************************/
  sc->scs = SCS_REG_VAL;                  // select clock range
 
  if((CLKSRCSEL_REG_VAL & CLK_SRC_SELECT_MASK) == CLK_SRC_MAIN)
  {
    sc->scs |= SCS_OSCEN;                 // enable main oscillator
   
    while((sc->scs & SCS_OSCSTAT) == 0) ; // wait for osc to stabilize
  }         

  /******************************* PLL 0 *********************************/
  sc->clksrcsel = CLKSRCSEL_REG_VAL;    // set pll 0 clock source
  sc->pll0cfg   = PLL0CFG_REG_VAL;      // set multiplier and divider bits
  sc->pll0con   = 0x01;                 // enable pll 0
  sc->pll0feed  = 0xAA;
  sc->pll0feed  = 0x55;
 
  sc->cclksel = 0x00000001;
 
  while(!(sc->pll0stat & PLL0STAT_PLOCK0)) ;// wait for pll to lock

  sc->cclksel  |= 0x00000100;
 
  sc->clkoutcfg = CLKOUTCFG_REG_VAL;
   
  if(CLKOUTCFG_REG_VAL & (0x00000001 << 8))
  {
    SET_GPIO_DIR_OUTPUT(127);
    SET_PINSEL(127, 4);
  }
}

标签 (1)
0 项奖励
回复
2 回复数

1,933 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Mon Oct 14 11:36:00 MST 2013
Hi,

Please ensure the following bits are set to operate at 120MHz for IAP command:

BOOST[1:0] =11 in register PBOOST
ROM_LAT =1 in register Matrix_Arb

Note that there is an error in the UM for the description of ROM_LAT.

ROM_LAT bit is set by the boot loader. However, in debug mode, some debuger bypass the bootloader - leaving this bit as 0. This bit should always be set to1 for any operation above 60MHz.

0 项奖励
回复

1,933 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri Sep 20 23:37:34 MST 2013
Hi,
Which part of the execution has issue with the 120mhz setting.
Thanks!
0 项奖励
回复