LPC1778 Full duplex

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1778 Full duplex

1,019 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akshimmu on Thu Apr 14 21:41:45 MST 2016
i have connected 2 LPC1778's for communication via uart1 in both the uC's. The TX of uart1 is connected to RX of uC2 and vice versa. Since LPC1778 has separate TX and RX blocks,does this setup support full duplex? That is, while uC1 is transmitting, uC1 can also receive from uC2?
Labels (1)
0 Kudos
Reply
1 Reply

1,004 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply