LPC1778 Full duplex

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1778 Full duplex

1,008件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by akshimmu on Thu Apr 14 21:41:45 MST 2016
i have connected 2 LPC1778's for communication via uart1 in both the uC's. The TX of uart1 is connected to RX of uC2 and vice versa. Since LPC1778 has separate TX and RX blocks,does this setup support full duplex? That is, while uC1 is transmitting, uC1 can also receive from uC2?
ラベル(1)
0 件の賞賛
返信
1 返信

993件の閲覧回数
lpcware
NXP Employee
NXP Employee
bump
0 件の賞賛
返信