LPC1778 EMC LQFP144, What are P5[0] EMC_A[24] и P5[1] EMC_A[25]

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1778 EMC LQFP144, What are P5[0] EMC_A[24] и P5[1] EMC_A[25]

1,120件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dfcbkbq on Sun May 04 21:25:48 MST 2014
Hello!

I try to connect 17-bit adress wide SDRAM to LPC1778 LQFP144. There only A0-A15 and A24,A25 are available on LQFP144. What are P5[0] EMC_A[24] и P5[1] EMC_A[25]? Can I use it to connect to EMC  in 17-bit wide adress mode?

Regards,
Vasilij.
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

1,105件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by MikeSimmonds on Sat Nov 08 05:54:06 MST 2014

Quote: xianghuiwang
H, Vaslilij,

There may be some inaccuracy in the DS, we will double check this and get back to you. I confirmed your observation, it seems suspicious.
Thanks,



I have not seen a posted reply from NXP
What was found in the 'double check'?

Mike.
0 件の賞賛
返信

1,105件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dfcbkbq on Mon Sep 22 05:57:25 MST 2014
So, I chacked it by myself. Yes there do. P5[0] EMC_A[24]  and P5[1] EMC_A[25] work like emc A[24] emc A[25]. So you can use it.
0 件の賞賛
返信

1,105件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Pacman on Tue Sep 09 05:12:01 MST 2014
I too am interested in this subject. I asked a similar question a long time ago (the answer is still pending)
0 件の賞賛
返信

1,105件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Dfcbkbq on Mon Sep 08 22:05:32 MST 2014
And???
0 件の賞賛
返信

1,105件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by xianghuiwang on Fri May 09 12:03:35 MST 2014
H, Vaslilij,

There may be some inaccuracy in the DS, we will double check this and get back to you. I confirmed your observation, it seems suspicious.
Thanks,
0 件の賞賛
返信