LPC176x RTC crystal and capacitor recommendations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC176x RTC crystal and capacitor recommendations

1,913件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by parikshitkr on Wed Dec 12 04:32:58 MST 2012
Hi,

In LPC1768 datasheet (rev 9) I see in section 14.2 guidelines on Crystal and load capacitor. For RTC I can not find a clear guideline on what crystal to use and load capacitor for it. Could you recommend should be crystal specs, i.e., something similar to Table 22.

regards
Parikshit
ラベル(1)
0 件の賞賛
返信
1 返信

1,489件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Daniel Widyanto on Wed Dec 19 00:31:00 MST 2012
Hi,

The RTC oscillator recommended 32kHz crystal to have:
- CL (Crystal Cap load): 11pf, Max Rs (Crystal series resistance) < 100kohm, Recommended external cap: 18pF (or)
- CL (Crystal Cap load): 13pf, Max Rs (Crystal series resistance) < 100kohm, Recommended external cap: 22pF (or)
- CL (Crystal Cap load): 15pf, Max Rs (Crystal series resistance) < 100kohm, Recommended external cap: 27pF

We'll feedback your input for the RTC xtal selection into User Manual. Thanks for bringing this up
0 件の賞賛
返信