LPC176x/5x user manual (UM10360.pdf) discrepancy (regarding three phase AC mode)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC176x/5x user manual (UM10360.pdf) discrepancy (regarding three phase AC mode)

3,160 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rons on Sat Jun 11 05:53:01 MST 2016
UM10360.pdf (Rev 3 - 19 December 2013 & Rev 3.1 -2 April 2014)

referencing Rev 3.1:


Section 25.7.8 MCPWM Dead-time register (MCDT) (page 544)
-------------------------------------------------------------------------------
DTO,DT1,DT2 used when ACMODE = 0
DTO used for all 3 channels when ACMODE = 1
-------------------------------------------------------------------------------
This makes sense because channel 0 timer is used for all 3 channels.



Section 25.7.8 Three phase AC mode (page 550)
--------------------------------------------------------------
ACMODE = 1

The dead-time mode is disabled.
--------------------------------------------------------------

NXP engiineer(s): What gives?
Labels (1)
0 Kudos
Reply
2 Replies

3,084 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

3,084 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by rons on Sun Jun 12 11:11:00 MST 2016
I will tell you what gives. A manual writer only types into a manual what he/she has been told.

The section 25.7.8 comment "The dead-time mode is disabled." is wrong.
0 Kudos
Reply