LPC176X RTC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC176X RTC

10,422 Views
769403396
Contributor I

lpc1764/1768 used RTC,时间走的误差很大,批量生产的板子,一个小时有几秒到几十秒的误差,也有走的比较准的,找不到原因,希望帮忙解决,谢谢!

TEL:13715155285,  QQ:769403396

0 Kudos
Reply
4 Replies

10,256 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, WangHui,

我认为外接32.768KHz晶体不准确导致时钟误差,你可以用频率计来测量晶体的输出来确定时钟误差。 得知误差后,你可以用calibration register 来校准。

Hope it can help you

BR

Xiangjun Rong

0 Kudos
Reply

10,254 Views
769403396
Contributor I

Hi,关于设备时间快慢的问题,在分析的时候,32768晶振及起振电容都做了更改和替换,问题依旧,但是更换LPC1764可以解决(有时更换后问题依旧,再次更换MCU就解决了),对时间快慢的设备,上周对电路做了更改,初步测试4h时间误差在1s~2s内,这周会进一步继续跟进分析,电路更改如下:

把二极管D6去掉,二极管D3使用0欧姆电阻代替,初步观察时间稳定,个人分析,设备在断电和上电时RTC供电电压不同,影响了RTC的稳定,所以时间出现了偏差。

还有一个问题,就是另外一款设备最先使用LPC1768片内RTC,现在出货一年多有余,发现整批设备断电在仓库存放一年时间,CR1220电池电量被耗完,所以怀疑片内RTC功耗比较大,希望可以帮忙分析跟进一下,LPC1764 datasheet上是小于1ua,按照1ua计算,CR1220 40maH的电池可以使用十几年,但是实际上一年时间电量基本被耗完,所以需要support一下。

0 Kudos
Reply

10,254 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Wang,

关于RTC的功耗, 你还要考虑二极管D3的功耗, C21的漏电以及电池本生的漏电及质量, 我不好说。但你可以测定VBAT 脚的电流。

BR

XiangJun Rong

0 Kudos
Reply

10,254 Views
769403396
Contributor I

Hi,你好,现在已经把BOM更改成:去掉D6,C21,D3由1N5819改为0欧姆电阻。车间维修用批量测试的时候,老化24小时,发现有些走的很准,大部分在正负5s误差内,有20%误差比较大(正负十几秒/几分钟/一个多小时的都有),遇到这种误差比较大的设备我已经给供应商(创达)了,希望尽快提供support,车间已经堆压了好多设备了,谢谢!

0 Kudos
Reply