LPC1769 worst case power consumption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 worst case power consumption

1,588 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Transient Rob on Wed Jun 08 12:01:54 MST 2016
Hello everyone,

Is there any data on the worst case power consumption for the LPC1769?  (Most likely at 85 Celsius, 120MHz with all blocks enabled/running, not counting any output current)
The datasheet only provides a typical case of 67 mA at 25 C, and I'm looking for the worst case in order to calculate holdup times for brief power interruptions. 

Thanks for any information you may have,

Rob
Labels (1)
0 Kudos
Reply
2 Replies

1,403 Views
lpcware
NXP Employee
NXP Employee
bump
0 Kudos
Reply

1,403 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by wmues on Thu Jun 09 01:40:26 MST 2016
If you get no official answer, I would double the typical case and calculate with this value, and then do a measurement with the real application.
0 Kudos
Reply