LPC1769 expresso board with baseboard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC1769 expresso board with baseboard

1,266 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Wed Jul 30 23:47:10 MST 2014
Hi,  I am uisng LPC expresso (LPC1769) board, base board and expresso IDE. I download the Free RTOS example and it is workign fine. I need to use RS232(not through USB) -DB9 to communicate to my deveice.

I look at the LPC17xx.cmsis.driver.library and look preety startight forward for bare metal programming,

Q1. Is there any example avaible to use UART0/1/2 driver from above and create a FreeRtos version of the Driver(API) ?


terry

Labels (1)
0 Kudos
Reply
2 Replies

1,239 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Keidy on Tue May 12 23:46:38 MST 2015

Hi! Terry

Please help with this problem i have the same issues.

I can not send data to Rs232, LPc1769 + LPC xpresso Baseboard + FreeRTOS

Thanks a lot
0 Kudos
Reply

1,239 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by terrype on Thu Aug 21 18:23:13 MST 2014
thanks terry, it is working now


terry
0 Kudos
Reply